AXIS#.PL.FB
Description
AXIS#.PL.FB returns the position feedback value. The value represents the feedback after the following operations have been performed:
- Homing offset ( AXIS#.HOME.OFFSET)
- User offset ( AXIS#.PL.OFFSET)
- Axis direction ( AXIS#.DIR)
- Position loop feedback gain ( AXIS#.PL.KFB)
- Modulo ( AXIS#.PL.MODP1, AXIS#.PL.MODP2) if modulo is enabled ( AXIS#.PL.MODPEN)
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read Only |
Units |
Rotary: counts, rad, deg, custom units, 16-bit counts See Position Units for details. |
Range |
Depends on units. See Position Range for details. |
Default Value |
N/A |
Data Type |
Float |
See Also |
|
Stored in Non-Volatile Memory |
No |
Variants Supported
Supported on all variants.
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
---|---|---|---|---|---|---|---|
AXIS1.PL.FB |
6064h |
00h |
Signed32 |
Position |
- |
Read only |
Yes |
AXIS2.PL.FB |
6864h |
00h |
Signed32 |
Position |
- |
Read only |
Yes |
Name |
ID |
Hex |
Data Type |
Access |
Units |
---|---|---|---|---|---|
AXIS1.PL.FB |
5904 |
1710 |
Signed32 |
Read Only |
Position |
AXIS2.PL.FB |
71440 |
1171 |
Signed32 |
Read Only |
Position |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
AXIS#.PL.FB |
5904 |
Signed32 |
Read Only |
Position |
Related Topics